Add, Edit, Reorder and Remove Layers on a Mimic

You can use the Layers button on the Mimic Properties window to access the Layers window for a Mimic. The Layers button is only available when you display the Mimic Properties window for an individual Mimic (rather than via the Options window).

You can use the Layers window to add, remove, and organize the layers on the current Mimic. For more information on the Layers window, see Layers.

Further Information

Defining the Default Mimic Properties for a Specific Mimic.


Disclaimer

Geo SCADA Expert 2021