Add Live Values to a Mimic

You can add ‘live’ values for any database item to a Mimic by either:

Example:

If you wanted to display the ‘live’ CurrentQualityDesc value of a point, you could display the OPC Data Bar, expand the property tags for the point, then select CurrentQualityDesc. With the property selected, you would then drag it onto the Mimic. Geo SCADA Expert creates a text box containing the ‘live’ CurrentQualityDesc value of the point and displays it on the Mimic.

When you have added a ‘live’ value to a Mimic, the value will update whenever the value changes in the database.

The text boxes, shapes, Lists and so on that are added to the Mimic when you drag and drop have animations in place. You can edit these animations to suit your own requirements as needed (see Animations).


Disclaimer

Geo SCADA Expert 2021