BackColour

The BackColour defines the background color of the embedded List. You can animate this so that it uses a color that is associated with a database item (such as the alarm color), refers to a custom color, or is set to a specific color (an RGB value).

This property works in a similar way to the FillColour except that it applies to the background of an embedded List instead of the fill of an object. However, this animation can be overridden by the Background column in an SQL query.


Disclaimer

Geo SCADA Expert 2021