Colour

The Colour property is used to define the color of the line/outline.

You can animate the Colour property in the same way as the FillColour property—the only difference is that the Colour property applies to the outline instead of the fill. For more information, refer to the Fill Animations section (see FillColour).


Disclaimer

Geo SCADA Expert 2021