To access the animation properties for an object, you need to display its Animations window. The Animations window contains a list of the animation properties that are available for the selected Mimic object and shows any expressions that are in place.
To display the Animations window:
- Display the Mimic object's Properties window by double-clicking on the Mimic object (with the Mimic in Design mode).
- Select the General tab.
- Select the Animations button.
Alternatively, right-click on the Mimic object and select the Animations option from the context sensitive menu.
For information on the Animations window settings, see Using the Animations Window.