Editing Objects on a Mimic

When you have added an object to a Mimic, you need to access its Properties window so that you can edit its settings (see Display the Properties Window for an Object on a Mimic). Each object's settings allow you to alter the appearance and functionality of each Mimic object.

The following topics in this section provide more information about the settings to which the various Properties windows provide access. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

For information on how to use the Color window to define custom colors, see Using the Color Window.


Disclaimer

Geo SCADA Expert 2021