Editing an Embedded X-Y-Z Plot

When you have added an embedded X-Y-Z Plot to a Mimic, you can access its Embedded X-Y-Z Plot Properties window to edit its settings. To display the window, double-click on the object on the Mimic. (For other ways of displaying the window, see Display the Properties Window for an Object on a Mimic.)

The Embedded X-Y-Z Plot Properties window has two tabs. For more information concerning each tab, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021