Making an Embedded Alarms List’s Default Filter Settings Take Precedence

You need to define the alarm filter manually if:

and

This is because the default settings have no need for Geo SCADA Expert to generate a string. So when Geo SCADA Expert merges the embedded Alarms List’s filter with that of a User account, the User account filter string is used. This is because the User account’s filter string has defined clauses whereas the embedded Alarms List’s filter is blank.

Embedded Alarms List Filter String User Account Filter String Result

String created manually by user

Blank

Geo SCADA Expert applies embedded Alarms List’s filter string

String created manually by user, every clause included

String created manually by user

Geo SCADA Expert merges the two filter strings and applies the resulting filter. If there is a conflict between the two filters, the embedded Alarms List’s filter takes precedence

String created manually by user, some clauses omitted

String created manually by user

Geo SCADA Expert merges the two filter strings and applies the resulting filter. If there is a conflict between the two filters, the clauses that are explicitly defined in the embedded Alarms List’s filter string take precedence. However, any clauses that are left out of the embedded Alarms List’s filter cannot take precedence.

Blank

Blank

Geo SCADA Expert displays an unfiltered embedded Alarms List (no filter is applied).

String created manually by user, some clauses omitted

Blank

The clauses which are specified in the embedded Alarms List’s filter string are applied. The default values for the clauses that are not specified in the filter string are also applied.

Blank

String created manually by user

The User account filter string is applied.

To configure the embedded Alarms List’s filter so that its default filter values take precedence over any User account filter strings:

  1. Display the Embedded Alarms List String dialog box (see Filter an Embedded Alarms List)
  2. On the Edit Embedded Alarms List String dialog box, select the ...browse button to display the Filter window.
  3. Using the Filter window’s settings:
    • Select the Only Show Alarms Assigned to Current User check box
    • Add a Source
    • Add an Area of Interest (if this feature is enabled on your system)
    • Change the Minimum Severity setting
    • Change the Maximum Severity setting
    • Clear at least 1 Category.
    • Select any State (that is,select any option other than All States).

    The reason for changing the settings from the default settings is that it forces Geo SCADA Expert to generate a string automatically. You can then edit the string so that the default settings are used in the string, and so, as a result will take precedence over the clauses in any User account filter strings.

  4. Select the OK button to confirm your selections.
    This closes the Filter window. As you have defined a filter, Geo SCADA Expert generates the corresponding string automatically and it is shown in the Edit Embedded Alarms List dialog box.
  5. Edit the string so that the default filter values are applied. Your string should appear like this:

    AOI="World"&Source="*"&MinSeverity="1"&MaxSeverity="1000"&Categories="Alarm Inhibit;Archive Volume;Archiving;Authentication;Callback;Channel Status;Control Status;Dial In Overactive;EFM Alarm;File Upload Status;Forecast;Interface Alarm;Off Scan;Outstation Comms;Outstation Error;Outstation Hardware;Pager Comms;Point Error;Point No Change;Point State;Scanner Status;Scheduled Dial In;Server Status;SMS PagerService;SNMP Configuration Error;System Alarm"&AlarmState="All"&Assigned="FALSE"

    To apply the default settings, you will need to adjust the values for several clauses: the value for the categories clause needs to include every category that is available on your system; the value for the AOI clause needs to be World (which includes every Area of Interest); the value for the MinSeverity should be 1 and the MaxSeverity should be 1000.

  6. Select the OK button to confirm your string and close the Edit Embedded Alarms List String dialog box.
    The default filter values are applied to the embedded Alarms List and will be applied whenever the embedded Alarms List is displayed.

Further Information

Alarm Filter Syntax: see Alarm Filter String Syntax in the Geo SCADA Expert Guide to Alarms.


Disclaimer

Geo SCADA Expert 2021