Using Context-Sensitive Menu Options on a Mimic

In ViewX and Virtual ViewX, when a Mimic is in Run mode, some options on the ribbon are also available as context-sensitive menu options.

The following options are available when the Mimic is in Run mode and you right-click on the Mimic:


Disclaimer

Geo SCADA Expert 2021