Using the Animations Window to Set Up Pick Actions

You can use the Animations window to set up pick actions. This is useful when you need the availability of a pick action to be dependant on a condition. For example, you can use an animation expression to set a pick action menu to only be available when a point is in a specific state.

There are several animation properties that relate to pick actions, including:

For more information on setting up the pick action animations, see Animations.


Disclaimer

Geo SCADA Expert 2021