Zoom Selection

You can use Zoom Selection to magnify a Mimic. The main advantage of the Zoom Selection over the other Zoom tools is that it allows you to specify which part of a Mimic is to be shown at an increased level of magnification.

To use Zoom Selection:

  1. Activate Zoom Selection:

    In ViewX, select the Zoom Selection command in the Navigation group on the Home tab.

    In Virtual ViewX, right-click on the background of the Mimic to display a context sensitive menu, then select the Zoom Box option.

  2. Draw a selection box over the area that you want to magnify.
    The area will be magnified when you release the left-hand mouse button.
  3. Repeat this procedure as required.

Disclaimer

Geo SCADA Expert 2021