Geo SCADA Expert Simple Modbus Driver

The Simple Modbus Driver can communicate with Modbus Slaves and Modbus PLCs using either:

With the Simple Modbus driver, you configure Scanners to determine which data gets polled at which frequency—the points on a Scanner are all polled at the same rate.

If your system has a simple configuration and the above functionality fulfills your system requirements, you can use either the Geo SCADA Expert Simple Modbus Driver, or the Geo SCADA Expert SCADAPack Modbus Driver to communicate with the Modbus devices on your system.

Refer to the rest of this guide for information on configuring Simple Modbus driver-specific items and features within Geo SCADA Expert.


Disclaimer

Geo SCADA Expert 2021