Configure the Basic Source Properties

Use the fields at the top of the Source tab to specify whether the source is functional, the channel that is used to transmit the source data, and the address of the device that is to scan this source for Modbus data:


Disclaimer

Geo SCADA Expert 2021