Configuring OPC Devices in Geo SCADA Expert

On a Geo SCADA Expert system, you configure the Geo SCADA Expert database so that entries in the database reference the devices and plant that you are trying to monitor on your system. This section summarizes the database items that you need to configure in order to read and write to data on other servers, using the OPC protocol.

In order to communicate with other servers using the OPC protocol, the Simple OPC Driver has to be installed and running on the Geo SCADA Expert servers on your system. The driver is represented by the OPC Client - Simple component in the Geo SCADA Expert Installation Wizard’s Setup window. The component is located within the Server branch of the tree that is displayed in the window (see Install a Driver in Geo SCADA Expert in the Geo SCADA Expert Guide to Drivers).

When you configure OPC items in the Geo SCADA Expert database, many of the settings for those items need to correspond to the settings on the relevant OPC servers on your system. You need to have access to, or a list of, these settings before you can configure the OPC database items successfully.

For instance, you need to know the read and write mechanisms that are supported by the OPC servers on your system, and the user names and passwords that allow the required level of access to the data on those servers.

You also need to be aware of which optional features are required for each OPC item. These features include:

You can also use core Geo SCADA Expert features with OPC database items, including Lists, Actions, and Mimics. See the core documentation for details.

For each OPC device, you need to configure:

  1. Simple OPC Server(s) to specify the servers on which data is to be scanned, along with any access and security settings required to communicate with those servers.

    You need to configure one OPC Server item in the database for each server with which you want to communicate using the OPC protocol (see Configuring a Simple OPC Server).

  2. Simple OPC Scanner(s) to specify which nodes are to be scanned and the rates at which the data is to be retrieved.

    You need to configure a minimum of one OPC Scanner per OPC Server. You can attach multiple scanners to the same server. For instance, you might configure different scanner to have different scan rates or offsets, in order to retrieve some data at different intervals or times to other data.

    For more information, see Configuring a Simple OPC Scanner.

  3. Simple OPC Points to represent the measuring instruments and control devices on the servers that are communicating using the OPC protocol.

    For more information, see Points Used on Simple OPC Scanners.

To minimize the time that it takes to configure the required OPC items, you may want to configure them in the order listed above, as the Scanner configuration requires that you specify a server, and point configuration requires that you specify a scanner, and so on.


Disclaimer

Geo SCADA Expert 2021