Define which Configuration Properties are Retrieved from an OPC Source

When a similar point property exists in an OPC data source, the Simple OPC driver can retrieve the value of that property directly from the OPC data source. Retrieving the value of a configuration property in this way avoids the need for engineers to specify the property manually within the Geo SCADA Expert database.

Use the Configuration Properties section of the OPC tab to specify which property values the Simple OPC driver is to retrieve for an analog point, and the IDs that identify each of those properties in the OPC data source. For further information on using this section of the tab, see Retrieve Configuration Properties From an OPC Data Source.

For an analog point, you can specify whether the Simple OPC driver is to retrieve the values for any of these properties:.



Disclaimer

Geo SCADA Expert 2021