Specify the Source Value of a Point

Each Simple OPC point in the Geo SCADA Expert database derives its value from an OPC source value. Use the fields in the Value section of the OPC tab to specify the type of source value from which this particular database point derives its value. Geo SCADA Expert processes the point data differently, according to the type of source value that the database point represents.


Disclaimer

Geo SCADA Expert 2021