Disable Switching

Associated with: OPC UA Subscription items

Security permission required to access this pick action: Switch Line

Use the Disable Switching pick action to stop an OPC UA subscription from being switched to use another OPC UA server in a multiple OPC UA server configuration.

Use the Enable Switching pick action to re-enable switching between servers.

If an OPC UA server fails or a subscription that is associated with an OPC UA server fails while switching is disabled, then automatic switching is blocked and the Switch Server pick action is disabled.

NOTE: If using this pick action with the Automation Interface, you have to specify the method name DisableSwitching.


Disclaimer

Geo SCADA Expert 2021