Refresh

Associated with: OPC UA Subscriptions and OPC UA Points

Security permission required to access this pick action: Retrieve Data

Geo SCADA Expert typically reads items for data on a scheduled basis. If required, you can use the Refresh pick action to read items on demand. Select the Refresh pick action to display the following window and request a current data update of the point or points that are associated with a particular OPC UA Subscription.

Select the pick action on a specific point to refresh the data for just that point. Select the pick action on an OPC UA Subscription item to refresh the data of the points on that subscription.

The pick action is only available on OPC UA Subscriptions and Points that are 'live' and in communication with an OPC UA server to which to which the Subscription relates.

NOTE: If using this pick action with the Automation Interface, you have to specify the method name Refresh.


Disclaimer

Geo SCADA Expert 2021