Use the WebX Interface

ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of Geo SCADA Expert. For information about the Virtual ViewX client that is supported by Geo SCADA Expert 2019 onwards, for which the web server is hosted using IIS, click here.

This section applies if your system is not customized to use default views.

You can use the links on the database web page (see Browse your Database on a WebX Client) to access different levels of the database—the database web pages correspond to the various levels in the Database Bar tree-structure in ViewX (see Database Bar).


The Parent group links to the group above the item or page that you are viewing.

The Children group contains items that are part of the group that you are viewing, for example points or Mimics that are part of a group.

 

You can perform these actions on a WebX client:

 

The Web browser remembers the order in which you have viewed WebX pages. The browser should provide buttons that allow you to move back and forth between the pages that you have been viewing. For example, Windows® Internet Explorer 11 allows you to:

 

Specific actions you can perform on a WebX client include:


Disclaimer

Geo SCADA Expert 2021