Using an Original WebX Client

ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of Geo SCADA Expert. For information about the Virtual ViewX client that is supported by Geo SCADA Expert 2019 onwards, for which the web server is hosted using IIS, click here.

You can use a web browser such as Microsoft Internet Explorer to access your system remotely. A PC that accesses the system via a web browser is called a WebX client. You can use a WebX client to access the operational features of Geo SCADA Expert, including alarm response features and controls. Your system’s security settings (user accounts, permissions, passwords and so on) also apply to WebX, and help to protect Geo SCADA Expert from unauthorized access by WebX clients.

WebX provides access to operator-level features. For configuration features, you need to use a ViewX client.

For the tutorial, you are going to access your system via Microsoft Internet Explorer, so you need to have this application installed on your PC. The minimum requirement is for Microsoft Internet Explorer 11. For information on Microsoft’s web browser applications, please refer to the Microsoft website at www.microsoft.com.

Original WebX uses Microsoft ActiveX Controls technology to display various types of document. ActiveX Controls are only supported by Microsoft Internet Explorer®. To access the suite of functions and types of display to which Geo SCADA Expert's web client and your user account provides access, we recommend that you use Internet Explorer 11 to run Original WebX. Other web browsers provide access to a sub-set of functionality and document types. The interface layout varies slightly between browsers. The Original WebX documentation in the online Help explains Original WebX functionality that is available using Internet Explorer 11.

If you haven’t completed the earlier sections of the tutorial, you will also need to import some configuration. The configuration comprises a collection of database items with which you can interact and use to generate values and alarms:

  1. Log On to ViewX as the user 'EngExample' (see Log on to your System).
  2. Display the Database Bar (see Display an Explorer Bar).
  3. In the Database Bar, right-click on the System icon then select Import from the context sensitive menu. This displays the Import From window.
  4. In Windows, browse to C:\Program Files\Schneider Electric\ClearSCADA\Tutorial Files.
  5. Select the SerialComms.sde file.
  6. Select the Open button to close the Import From window and import the file.
  7. Repeat this process, only instead of importing the SerialComms.sde file, import the following files:
    • MyFirstTest.sde
    • SiteTemplate.sde
    • SiteABCInstance.sde
    • SiteDEFInstance.sde

When you have installed the relevant Internet Explorer software on your PC and you have imported the configuration (if required), you can proceed to access your system via the web interface:

  1. Display the WebX Interface.
  2. Log on to the System via WebX.
  3. Use the Navigation Tools to Access other Displays.
  4. Access Database Items via WebX.
  5. Display a List of System Alarms via WebX.
  6. Display a List of System Events via WebX.
  7. Display a Queries List via WebX.
  8. If you are automatically logged off when using WebX, you should log back on as the 'EngExample' user.


Disclaimer

Geo SCADA Expert 2021