Define the Set Clock Method

Use the Set Clock Method field on the SCADAPack tab to define whether a controller’s clock is synchronized from Geo SCADA Expert or another source:

The options vary, depending on the type of controller:

For information about any Set Clock Method options not mentioned above, see the appropriate SCADAPack Modbus extension driver guide.


Disclaimer

Geo SCADA Expert 2021