Points Used on SCADAPack Modbus Controllers

SCADAPack controllers support a combination of these point types:

You need to configure one point of the appropriate type per point on a controller. You configure the properties for each point using the appropriate SCADAPack Modbus Point Form.

The rest of this section covers the configuration of properties that are common to most points supported by the SCADAPack Modbus driver. It includes information on how to:

For information on the minimal amount of configuration that you can undertake to produce a functional SCADAPack point in Geo SCADA Expert, see Minimum Configuration.

In addition to the points listed above, Geo SCADA Expert can support other types of point, using the SCADAPack Modbus Realflo Extension Driver. For information on SCADAPack Modbus points not listed above, see the Geo SCADA Expert Guide to the SCADAPack Modbus Realflo Driver.


Disclaimer

Geo SCADA Expert 2021