Scanning Direct Controllers on the SCADAPack Modbus Driver

This topic describes how to configure the SCADAPack Modbus driver to scan (poll) SCADAPack Direct controllers for data. Use this information in conjunction with the advanced drivers scanning information (see Scanning Direct Outstations in the Geo SCADA Expert Guide to Advanced Drivers).

To determine how the SCADAPack Modbus driver scans SCADAPack Direct controllers, configure the following:

Also see Specify how any Scanning Gaps are Handled.


Disclaimer

Geo SCADA Expert 2021