Supported Realflo Flow Computer Versions
Except where stated otherwise for specific features, this driver provides support for functionality that is available in SCADAPack Modbus Realflo devices that are running Flow Computers up to and including the following version(s):
7.02.1
The earliest version of the Realflo Flow Computer with which the driver is compatible is 5.20.
For more comprehensive information about Realflo and Geo SCADA Expert cross-compatibility, see the Cross-Compatibility page on our Geo SCADA Knowledge Base website. (The page also includes information about ClearSCADA, the name by which Geo SCADA Expert was formerly known.)