Density Properties (Liquid Flow Run)

The fields within this section of the Liquid tab display those properties that are associated with Density measurement.

You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).

The input alarms section of the Density section allows you to set the alarm thresholds for alarm types that have been enabled in the Inputs section of the Flow Run tab.

Use the following to configure alarm limits in the Density section:

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

Geo SCADA Expert 2021