Event Log Demand Poll

Associated with: SCADAPack Modbus Flow Runs

Security permission required to access this pick action: Retrieve Data

Use this pick action to request the driver to perform an Event Log Demand Poll on a controller for the events that are associated with a particular Flow Run.

  1. Select the Event Log Demand Poll pick action to display the Event Log Demand Poll window.
  2. Use the window’s Range field to specify which events to retrieve:

    • New—Retrieve only those events that have been raised since the last Event Log Demand Poll.
    • All—Retrieve all of the Flow Run’s events from the controller’s event log.

      Retrieving All of a Flow Run’s events may result in duplicate entries being logged in Geo SCADA Expert ’s Event Journal.


Disclaimer

Geo SCADA Expert 2021