Flow Calculation Properties (Gas Flow Run)

The Flow Calculation tab on the Flow Run Form displays the parameters that are associated with a Gas Flow Run’s flow calculation. You can use the fields to configure or view specific properties that are associated with the calculation.

The fields vary, depending on the The Type of Gas Flow Calculation that a Gas Flow Run performs.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021