Maximum Flow Runs Available

Associated with: Realflo controllers

This attribute indicates the maximum number of Flow Runs that the controller can support. The number is limited by the controller hardware and the Realflo license. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller.

Example:

2


Disclaimer

Geo SCADA Expert 2021