PEMEX Units

PEMEX units are used for gas flow runs on PEMEX controllers that are running Realflo version 6.7 or later. The Units column shows the measurement units. The Realflo Display column shows how these units are displayed on the screen and in printed reports.

Parameters and Values Units Realflo Display
Pipe and Orifice Diameters inches inches
Static, Base and Atmospheric Pressure psi psi
Differential Pressure inches H2O at 60 °F inches H2O at 60 °F
Flowing and Base Temperature °F °F
Viscosity centipoise cP
Density lbm/ft3 lbm/ft3
Mass lbm lbm
Mass Flow Rate lbm/hr lbm/hr
Volume MMCF MMCF
Volume Flow Rate MMCF/day MMCF/day
Heating Value BTU(60)/ft3 BTU/ft3
Energy Giga calories Giga calories
Energy Flow Rate Giga calories/day Giga calories/day
Flow Extension (Method 1) kg/m2s kg/m2s
Turbine Rate (volume) pulses/ft3 pulses/ft3
Turbine Rate (mass) N/A N/A
Altitude feet feet

The prefix M above units stands for thousands. The prefix MM above units stands for millions.

Be aware that 'M' in Metric and SI units represents a different quanitiy to that stated above.


Disclaimer

Geo SCADA Expert 2021