Points Used on SCADAPack Modbus Realflo Controllers

SCADAPack Modbus Realflo controllers support a combination of these point types:

To process other data on a Realflo controller, you use the appropriate ‘standard’ point type listed below:

For information on the minimal amount of configuration that you can undertake to produce a functional Realflo point in Geo SCADA Expert, see Minimum Configuration.

Be aware that although Geo SCADA Expert assigns Realflo Analog Input point addresses automatically, you need to manually assign appropriate addresses for those SCADAPack Modbus points that represent data other than Realflo data on a Realflo controller (see SCADAPack Modbus Realflo Point Addressing).


Disclaimer

Geo SCADA Expert 2021