SI Units

SI units are used for gas flow runs. The Units column shows the measurement units. The Realflo Display column shows how these units are displayed on the screen and in printed reports.

Parameters and Values Units Realflo Display
Pipe and Orifice Diameters m m
Static, Base and Atmospheric Pressure Pa Pa
Differential Pressure Pa Pa
Flowing and Base Temperature °K °K
Viscosity Pa-s Pa-s
Density kg/m3 kg/m3
Mass kg kg
Mass Flow Rate kg/s kg/s
Volume m3 m3
Volume Flow Rate m3/s m3/s
Heating Value J/m3 J/m3
Energy J J
Energy Flow Rate W W
Flow Extension (Method 1) kg/m2s kg/m2s
Turbine Rate (volume) pulses/m3 pulses/m3
Turbine Rate (mass) pulses/kg pulses/kg
Altitude meters meters
Velocity
(available from Realflo 7.02.1 onwards)
m/s m/s

Disclaimer

Geo SCADA Expert 2021