Temperature Properties

The fields within this section of the Flow Run tab display those properties that are associated with a Flow Run’s Temperature inputs.

You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).


The input alarms section of the Temperature section allows you to set the alarm thresholds for alarm types that have been enabled in the Inputs section of the Flow Run tab.

Use the following to configure alarm limits in the Temperature section:

The Temperature section also includes this property:

  • Constant—Set a constant value for the temperature property for the Flow Run. This setting is available only when the Input Type is set to Constant (available from Realflo 6.96 onwards).
  • Further Information

    For more detailed information on these properties, see the documentation provided with the Realflo application.


    Disclaimer

    Geo SCADA Expert 2021