Two-Phase Detection (Liquid Flow Run)

The fields within this section of the Liquid tab display those properties that are associated with Liquids measurement.

You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).

The following two fields are available if you select the Realflo Algorithm Detection type:

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

Geo SCADA Expert 2021