Configure a Modbus Point Scanner
You have to create a separate database item for each Modbus Point Scanner that is associated with a Modbus Slave Device item. When you have created a SCADAPack x70 Modbus Point Scanner item, use the Modbus tab to configure the scanner configuration.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.