SCADAPack x70

Configure the Event Attributes

The SCADAPack x70 tab on the Forms of SCADAPack x70 Counter Configuration items contains an Event Attributes section. Use the section to specify the counter's limit value. Also use the section to define the circumstances in which the SCADAPack x70 device generates point value-related events and/or alerts (alarms) for the item. The ability to generate alerts only applies when using a communications protocol that supports, and is configured to enable, event generation.

The section includes these properties:

For SCADA masters that are using the DNP3 protocol to communicate with the SCADAPack x70 device, the Unsolicited Events (DNP3 Only) field only applies when the relevant 'Master Point Data Class' is set to Class 1, 2, or 3 Event on the SCADAPack x70 Counter Configuration item's DNP3 tab (see Specify the Point Data Class used for DNP3 Communications).

Further Information

Multiple Alarm Limits.


Disclaimer

Geo SCADA Expert 2021