Configure the Device Options
The Settings tab on the Forms of SCADAPack x70 Device Configuration items includes a Device Configuration Options section. Use the section to select the roles and the associated functions that the selected device type supports. You can add or remove roles for the device at any time, for example, the device is operating as a DNP3 Slave and you want it to operate as a Modbus RTU Slave as well.
communication loss
SCADAPack x70 device can be configured to perform any of the following roles:
- Modbus IP Servers—A Modbus IP Server (slave) that reports information to a Modbus IP Client
- Modbus IP Clients—A Modbus IP Client (master) that requests information from Modbus IP Servers
- Modbus RTU Slave—A Modbus RTU Slave that reports information to a Modbus RTU Master
- Modbus RTU Master—A Modbus RTU Master that writes or reads Modbus register data from Modbus RTU Slaves
- DNP3 Slave—A DNP3 Slave that reports events to up to 3 DNP3 Masters
- DNP3 Router—A DNP3 Router between any combination of serial and Ethernet ports
- DNP3 Peer to Peer Master—A DNP3 Peer to Peer Master communications device that writes or reads DNP point data from a DNP3 slave
- DNP3 Data Concentrator Master—A DNP3 Data Concentrator Master that requests events from DNP3 Slaves
- IEC 60870-5-104 Controlled Station—Defines whether the IEC 60870-5-104 Server function is enabled. When enabled, the SCADAPack x70 device's IEC 60870-5-104 Controlled Station reports data to its controlling station(s).
- Slave Address(es) in Logic Editor Custom Field—A custom field that defines whether Slave addresses are displayed in the logic editor
- Realflo Flow Computer—Defines whether the Realflo Flow Computer function is enabled
The roles determine which configuration parameters are available for the device.
Clear both the Modbus RTU Slave and Modbus IP Server check boxes if the SCADAPack x70 device is not operating as a Modbus Slave and so is not using the Modbus protocol to communicate with its SCADA Master. Clearing both of these check boxes also prevents Geo SCADA Expert from downloading the settings that appear on the Modbus tab of the Analog, Digital, and Counter Configuration items that are associated with the SCADAPack x70 Device Configuration item. (When both check boxes are clear, the settings on the Modbus tab are ignored, regardless of whether that tab is enabled or disabled on the configuration Forms of the Analog, Digital, and Counter Configuration items.)