SCADAPack x70

Define Configuration Parameters for a Slave Device

The Configuration section of the DNP3 tab allows you to define the configuration parameters for a DNP3 Slave device.

Poll Limit

The number of unsuccessful polls before the remote device is considered to be offline.

Default: 2 unsuccessful polls.

Application Timeout

The timeout that is applied to application layer messages, such as class poll requests, that are sent to this DNP3 Slave.

Default: 60 seconds.

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

Health Poll Rate

Specify the rate at which the data concentrator attempts to poll this remote outstation, should the remote fail. The remote is deemed to have failed if its Poll Limit is reached (see above).

Default: 120 seconds.

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

Health Poll Type

Use this combo box to specify the type of message that the SCADAPack x70 should send to this remote slave device, in order to re-establish communications once the remote slave device has recovered from any failure. The SCADAPack x70 sends the selected poll type to the Slave device at the Health Poll Rate. Choose from:

Delay Measurement

This option has the smallest request and response size and is therefore the default option. Unless the DNP3 Slave does not support the Delay Measurement request type, select this option in preference to the others, if communications are to be checked with many remote devices simultaneously. This reduces the load on the communications network and the SCADAPack x70.

Class 0 Poll

The SCADAPack x70 sends a request for this remote device’s Class 0 static (current value) data.

Since a Class 0 poll returns static data for every DNP3 point on the DNP3 Slave, this option has the potential to return a high volume of data. High traffic volumes can disrupt network communications. This option is typically only recommended for DNP3 Slaves with a small number of DNP3 points and no events.

Event Poll

The SCADAPack x70 sends a request for any Class 1, 2, and 3 event data that is stored in this remote outstation’s internal Event Buffer(s).

Multiple Fragment Response

Select this check box if the remote slave device can send multiple fragment responses.

Clear the check box if the remote slave device does not support multiple fragment responses. The SCADAPack x70 will send a further Integrity poll request to the remote device whenever it receives a full fragment poll response with no DNP3 Class Data Available IIN bit(s) reported. The SCADAPack x70 is deemed to have retrieved all of the static (current value) data from the remote device once it has received two consecutive application fragments in which no DNP3 Class Data Available IIN bits are set.

Set Time

Select this check box if the SCADAPack x70 is to set the clock in this remote outstation whenever its DNP3 Need Time IIN bit is set.

Ensure the check box is clear if the remote outstation’s clock is to be set by other means. We recommend that the check box be left clear if the Poll Type is set to Static Only Poll, .


Disclaimer

Geo SCADA Expert 2021