SCADAPack x70

Description

Associated with: SCADAPack x70 Firmware Image items

This status attribute indicates the Description that was entered for the binary firmware image file when it was imported into the Geo SCADA Expert database (see Import Firmware Image).

Use this status attribute in conjunction with the File attribute to ascertain information about the .biz file with which this particular Firmware Image item is associated.


Disclaimer

Geo SCADA Expert 2021