SCADAPack x70

Device Configuration Serial Port Tabs

You use the Serial Port tabs on a Device Configuration item to specify the required Port Function and the settings associated with that port function.

The number of Serial Ports and their associated Port Functions differs, depending on the type of SCADAPack x70 device.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

 


Disclaimer

Geo SCADA Expert 2021