SCADAPack x70

Import/Upload Summary

Associated with: SCADAPack x70 Device Configuration items.

The Import/Upload Summary status attribute provides a summary of the latest import of a configuration file from RemoteConnect, or upload of the configuration from a SCADAPack x70 device.

There are three different stages of an import/upload transaction. The Import/Upload Summary status attribute displays different values at each stage:

Use this status attribute alongside the Import/Upload Status status attribute to monitor the progress of an import/upload transaction.

Further Information

For further information about the activities that occur when an import or upload is in progress, see the following topics:


Disclaimer

Geo SCADA Expert 2021