SCADAPack x70

Number of I/O Modules

Associated with: SCADAPack x70 Device Configuration items.

The Number of I/O Modules status attribute indicates the number of SCADAPAck x70 I/O Modules that are associated with the selected SCADAPack x70 Device Configuration item. You use this status attribute to determine the number of I/O Modules that are currently associated with, and/or can still be associated with, the SCADAPack x70 Device Configuration item within the given limit. If there are no associated I/O Modules, the status attribute displays the value '0'.

For more information about the maximum number of I/O modules that can be safely attached to each SCADAPack x70 device, see the Installation section of the respective Hardware Manuals in the documentation provided with the SCADAPack RemoteConnect software.

For information about I/O Modules, see Configure I/O Modules.


Disclaimer

Geo SCADA Expert 2021