SCADAPack x70

Number of Modbus Slave Devices

Associated with: SCADAPack x70 Device Configuration items.

The Number of Modbus Slave Devices status attribute indicates the number of SCADAPack x70 Modbus Slave Device items that are associated with the selected SCADAPack x70 Device Configuration item. You use this status attribute to determine the number of Modbus Slave Device items that are currently associated with, and/or can still be associated with, the SCADAPack x70 Device Configuration item within the given limit. You can add a maximum of 150 Modbus Slave Device items to a SCADAPack x70 device. If there are no associated Modbus Slave Device items, the status attribute displays the value '0'.

For information about Modbus Slave Devices, see Configure a Modbus Slave Device.


Disclaimer

Geo SCADA Expert 2021