SCADAPack x70

Number of Object Browsers

Associated with: SCADAPack x70 Device Configuration items.

The Number of Object Browsers status attribute indicates the number of Object Browsers that are associated with the selected SCADAPack x70 Device Configuration item. This status attribute is used to determine the number of Object Browsers that can still be associated with the SCADAPack x70 Device Configuration item within the given limit. If there are no associated Object Browsers, the value of this status attribute displays '0'.

For information about Object Browsers, see Configure an Object Browser.


Disclaimer

Geo SCADA Expert 2021