SCADAPack x70

Specify the Alert Notification Requirements

The SCADAPack x70 tab on the Forms of SCADAPack x70 Counter Configuration items contains an Alert Notifications section. Use the section to specify whether the SCADAPack x70 device is to store and report events and/or alerts (alarms) for the item.

The properties only apply when using a communications protocol that supports, and is configured to enable, event generation.

The section contains the following property:


Disclaimer

Geo SCADA Expert 2021