SCADAPack x70

Specify the Scaling Applied by Geo SCADA Expert

The Analog Point tab on the Forms of SCADAPack x70 DNP3 Analog Points contains a Scaling section. Use the section to define the scaling that Geo SCADA Expert is to apply to the analog values that are reported by the SCADAPack x70 device.

The scaling that is applied in Geo SCADA Expert is in addition to the scaling that is applied in the SCADAPack x70 device itself. The latter scaling is configured using the separate Scaling section on the Form of the SCADAPack x70 Analog Configuration item with which the Analog Point is associated (see Specify the SCADAPack x70 Device's Point Scaling). The Analog Point inherits those Scaling settings from the Analog Configuration item - you can view the settings in the SCADAPack Scaling section of the Analog Point's Form.

You use the Multiplier and Offset fields within the Scaling section to define whether any additional scaling conversion is applied to the analog's values in Geo SCADA Expert. For example, to convert values reported by the SCADAPack x70 device in Celsius into values in Fahrenheit for use in Geo SCADA Expert.

The Scaling section contains these properties:

In the following example, scaling is applied by Geo SCADA Expert to convert temperature from a Celsius value to a Fahrenheit value.

 

An Analog Point on a SCADAPack x70 device is measuring temperature in degrees Celsius. The temperature needs converting to Fahrenheit for use in Geo SCADA Expert. To convert degrees Celsius into degrees Fahrenheit, you multiply the Celsius value by 1.8 and then add 32 to the resultant value. In Geo SCADA Expert, this calculation is specified using the Multiplier and Offset fields in the Scaling section of the point's Analog Point tab.

Various properties take into account any Master Station Scaling that is applied. For example, the Alert Clear Value Deadband property on the Analog Point tab. This is a special case in which only the Multiplier is applied to the Alert Clear Value Deadband that the analog point inherits from the Configuration item (see Alert Notifications).

The Limit values in the Alarm Limits section of the Analog Point tab on the SCADAPack x70 DNP3 Analog Point also take into account any Master Station Scaling that is applied. The Multiplier and Offset are applied to the Limit values that the point inherits from the Alarm Limits section on the Form of the SCADAPack x70 Analog Configuration Item with which it is associated (see Configure the SCADAPack x70 Device's Alarm Limits Settings). For example, if the 4 High Limit value on the Form of the SCADAPack x70 Analog Configuration item is 10° Celsius, this gets scaled to 50° Fahrenheit for the 4 High Limit value on the Form of the SCADAPack x70 DNP3 Analog Point with which the Analog Configuration Item is associated.


Disclaimer

Geo SCADA Expert 2021