SCADAPack x70

UpdateIPRulesRowDetails

Associated with: SCADAPack x70 IP Whitelist Tables (on SCADAPack x70 Device Configuration items)

Security permission required to access this method: Configure

A whitelist table it used to specify what IP traffic is permitted to leave or enter the SCADAPack x70 device. Use UpdateIPRulesRowDetails to define the services whose traffic is permitted.

This method is the equivalent of updating the row properties within ViewX see Add and Configure the Entries in an IP Whitelist Table

Use these arguments for updating a row in the IP Whitelist table in the Geo SCADA Expert database.

WARNING

communication loss

Omission of IP addresses that are used by Geo SCADA Expert can lead to loss of communication between Geo SCADA Expert and your SCADAPack x70 device. Similarly, omission of IP addresses that are used by other devices with which the SCADAPack x70 device is expected to communicate can lead to loss of communication between the SCADAPack x70 device and those devices.
Verify that the required IP addresses are included in the IP Whitelist Table and that the specified settings are valid for the device and your network.
Failure to follow these instructions can result in death or serious injury.

Disclaimer

Geo SCADA Expert 2021