Configure Integer and Cardinal Point Scaling

Use the fields within the Scaling section of the <Point Type> tab to configure an SNMP Integer or Cardinal Point’s scaling. The SNMP driver applies the scaling to each integer or cardinal value that it retrieves from an SNMP agent, before passing the resultant value to the Geo SCADA Expert database. The driver applies the scaling in reverse whenever the Set Value pick action is used.


Disclaimer

Geo SCADA Expert 2021