Configure the Poll and Link Status Properties

If the point is used to retrieve Link Status, or current point data (as opposed to Trap notifications), you need to specify the poll properties in the Poll/Link Status section of the <Point Type> tab.

The fields within the Poll/Link Status section of the <Point Type> tab are only available for use when the point Action is set to Poll or Link Status(see Configure the Common Point Properties).


Disclaimer

Geo SCADA Expert 2021