Minimum Configuration

For a SNMP point to be capable of functioning, as a minimum you have to specify these features on the <Point Type> tab:

If you want point data to be stored historically, you also need to:

Also ensure that the point is In Service, and has saved, valid configuration. This will produce a point that is capable of functioning using the default configuration settings.

Note: For SNMPv2 and SNMPv3, points must be linked to a SNMP device. If you require SNMPv3 security you will need to create and configure an SNMP Device and associate the point(s) with the device.

see Create an SNMP Device


Disclaimer

Geo SCADA Expert 2021