Conditions.bool-primary-in

Determines whether a given value matches any value in a query or a list

Format

expression [ NOT ] IN ( { query-expr | expr-list } )

Remarks

Determines if the value of the expression matches one of the values in either the result set from a query or a comma separated list.

If an item in the list is an array then determines if the value matches an element in the array.

Expression IN ( QueryExpr )

is the same as

Expression = ANY ( QueryExpr )

Expression NOT IN ( QueryExpr )

is the same as

Expression <> ALL ( QueryExpr )

Example:

SELECT Name FROM Customers WHERE Country IN ('UK', 'USA', 'Germany')


Disclaimer

Geo SCADA Expert 2021